Avnet Silica’s Renesas Visible things Industrial Starter Kit Giveaway

Avnet Silica’s fully integrated IoT Platform is your complete solution from edge to enterprise

Simplify and secure your IoT solution with Avnet Silica’s complete evaluation and reference platform, Visible Things. It connects smart devices right to the cloud and enterprise software, and supports an ever increasing range of sensor, connectivity, gateway and security technologies. Together with Avnet Silica’s cloud, analytics, mobile and enterprise integration services, it’s a complete solution from edge to enterprise – so relax.

    Button - Buy Now -

Avnet Silica’s Visible Things Industrial Starter Kit provides a turnkey solution based on the Renesas Synergy™ Platform, that allows you to start designing at the API level and is equipped to handle an outstanding range of connectivity tasks.

Header       Header

Visible Things – Key Features

Sensor to server security layer on top of network security
Quick evaluation of end application
Highest degree of flexibility
Reduces development time significantly – time saving
Optimised power consumption
Cloud ready

Renesas Synergy™ Platform – Key Elements

Qualified commercial-grade software with a common API
Scalable and compatible ARM Cortex-M based microcontrollers
Intuitive professional development tools and kits
Time-saving end-to-end solutions
Click-through licensing plus a collection of specialized add-on software

Latest Power Management ICs from Ricoh

   

Ricoh have introduced new power management ICs to their latest product selection.

RP604 300 mA Buck-Boost DC/DC Converter for IoT applications

This product is in particular suitable in case a supply voltage is required which is somewhere in between the voltage level of a fully charged and fully discharged battery. At a certain moment the DC/DC Converter needs to switch over from Buck to Boost mode automatically. The RP604 is designed for IoT applications which are mainly in a sleep mode and wake-up periodically to perform a measurement, transmit some data and resume to sleep mode again. For such kind of applications, the current consumption in sleep mode should be kept as low as possible. The RP604 consumes only 0.3 µA and has a peak efficiency of 90% at 0.1 mA output current.

RP511 100mA Buck DC/DC converter for IoT applications 

The RP511 is a VFM buck DC/DC Converters with synchronous rectification which can be powered from a coin cell to a USB port. The smallest solution requires only 8.0 mm2 PCB area including three external components. Therefore, this product is highly suitable for small wearable applications such as smartwatches, fitness trackers, RF modules, sensor devices etc. Current consumption is only 0.3 µA and peak efficiency is at 95% at 0.1 mA.

More information can be found in the links provided below:

https://www.e-devices.ricoh.co.jp/en/products/power/dcdc/rp604/

https://www.e-devices.ricoh.co.jp/en/products/power/dcdc/rp511/

        

 

Visible Things Industrial Starter Kit in Stock Now with Avnet Silica

Visible Things

Visible Things simplifies the complexity of secure edge to enterprise IoT technology. It delivers a complete evaluation and reference platform to connect smart devices right through to the cloud and enterprise software. Avnet Silica supports an ever increasing range of sensor, connectivity, gateway and security technologies, together with cloud, analytics, mobile and enterprise integration services. Avnet Silica regularly add new features, provide updates and deliver training on their Visible Things platform.

Avnet Silica are giving away 10 Industrial Starter Kits worth 329€, so be quick and register here to win!

Visible Things Industrial Starter Kit

Meet Avnet Silica at Electronica for Advanced IoT and Automotive Solutions

Avnet Silica invites you to Electronica 2016

From 8 – 11 November 2016, the world’s leading trade fair for electronic components, systems and applications opens its gate again in Munich, Germany. Avnet Silica will showcase its advanced solutions for the Internet of Things (IoT) and automotive development.

On Avnet Silica’s main booth, they will present three demonstrations that highlight the power and flexibility of the Visible Things IoT platform – including embedded vision, security and cognitive analytics. Their automotive showcase will reinforce the next revolution in this growing industry, and show how customers can stay ahead of the curve in fast-developing areas such as autonomous vehicles, the connected car, security and eMobility. In addition, Avnet Silica will show a broad range of development boards and design tools, including development platforms for software-defined-radio, HMI, industrial computing, WiFi and IEEE 802.15.4 systems.

avnetbanner-728x90px

In Hall A4, Booth 179, you will have the opportunity to see demonstrations for Avnet Silica’s Visible ThingsTM IoT platform, which delivers rich functionality from edge to enterprise with outstanding cost, power and size specifications. On show for the first time will be a brand new gateway product focused on the industrial space, and a unique security architecture that delivers true enterprise-grade security from the IP network core all the way to smart sensor configurations at the network edge – including low-power non-IP-based sensors. The third demonstration, an embedded vision system, combines image capture from low-cost non-intelligent sensors with high-end cognitive analytics in the cloud, to deliver a uniqueIn combination of real-time analysis and long-term business intelligence.

You can visit the OEMsecrets.com team at Hall A4, Booth 122 to view all the latest pricing and inventory availability from Avnet Silica.

Whether it’s for an expert talk with their technology specialists or a friendly chat with the team, you are welcome to meet Avnet Silica and OEMsecrets at Electronica in Munich!