Learn all about Texas Instruments’ comprehensive Power Management porfolio

Simplify your DC/DC design with LMZM33603

The LMZM33603 36V, 3A power module offers stellar EMI performance in a compact QFN package.
Order yours today and enjoy the peace of mind that comes with reliable performance, small solution size, and reduced design cycle time.

Power your processor with the industry’s first 5+3- phase PMBus controller


Powering high-current processors requires flexible solutions, and the TPS53681 PMBus multiphase PWM buck controller delivers with dual output 6+2/5+3 phase configuration. This multiphase driverless controller is paired with TI smart power stages for accurate current sensing and excellent thermal performance.

The next generation of TVS surge diodes is here


With a 94% smaller footprint, lower leakage and flat-clamping technology, TI’s Flat-Clamp portfolio provides more robust protection than traditional TVS surge diodes.

TI’s new TVS3300 family of Flat-Clamps gives designers precise control over clamping voltage vs surge current, even across temperature. It’s time to re-evaluate your TVS protection. Learn more in the whitepaper.

NEW: Industry’s smallest 8A single-rail module


Powering your 4A to 8A digital load just got smaller, easier, and more reliable. At 7.5mm x 7.5mm, the TPSM84824 17V, 8A step-down power module provides the smallest footprint in its class. And with TurboTrans™ technology, it delivers fast transient response with the industry’s lowest overshoot.

TPSM84824 comes with minimal external components, and pin- and footprint-compatible 4A and 6A alternatives.

Introducing TI’s first PMBus power module


Presenting an easier way to power your high-current digital core: TPSM846C23 is a PMBus-compliant DC/DC power module with an integrated inductor and FETs that crams 35A of output current capability into 240mm2. Two of these modules can easily be paralleled to deliver up to 70A of output current to the point-of-load from a nominal 12V or 5V input voltage.

Save space in your automotive design with TI’s synchronous buck-boost DC-DC converter


The TPS5516x-Q1 family provides a cost-effective single chip solution for a regulated output voltage between 5V and 12V, with up to 1A load current depending on voltage requirements. The buck-boost overlap control ensures automatic transition between step-down and step-up mode with optimal efficiency.
These buck/boosts provide a smaller solution size and higher efficiency than a discrete boost-buck converter solution.

Highest efficiency and lowest standby power without the audible noise


Want the lowest standby power? Need to simplify your system design for your AC/DC applications? Get to know our newest power factor correction (PFC) controller, UCC28056. With zero cross detection scheme (without auxiliary winding) and advanced burst mode, UCC28056 will help you design your next offline system.

6A three-level buck battery charger enables faster charge times for portable electronics


TI’s BQ25910, the industry’s first integrated 6A three-level buck battery charger, is a game-changer for how we will charge our smartphones, tablets, electronic point of sale (EPOS) and other portable electronics in the future. New power conversion technology reduces battery charging time up to 50% and allows for up to 5% efficiency improvements compared to conventional architectures.

Get great EMI and thermal performance the easy way


Any engineers out there looking for high-efficiency DC/DC conversion without the headaches that typically come with EMI mitigation and thermal management? Everyone? Ok, good.

Introducing the LM73605/6 and LM76002/3 families of wide VINsynchronous buck converters. Designed with high integration, thoughtful pin-out, and best-in-class thermal coefficients, LM73605/6 and LM76002/3 give you amazing performance without all of the headaches.

The world’s smallest 36V, 1A DC/DC solution


With a 27mm2 package size and only two external components, the LMZM23600/ 01 power module can convert a nominal 24V input to 3.3V in a solution size that is 45% smaller than competition. With the simplicity of power modules paired with the magic of WEBENCH®, you can bring the world’s tiniest 36V, 1A buck design to market with blazing speed.

To find the best price for Texas Instruments search OEMsecrets

Latest Power Management ICs from Ricoh

   

Ricoh have introduced new power management ICs to their latest product selection.

RP604 300 mA Buck-Boost DC/DC Converter for IoT applications

This product is in particular suitable in case a supply voltage is required which is somewhere in between the voltage level of a fully charged and fully discharged battery. At a certain moment the DC/DC Converter needs to switch over from Buck to Boost mode automatically. The RP604 is designed for IoT applications which are mainly in a sleep mode and wake-up periodically to perform a measurement, transmit some data and resume to sleep mode again. For such kind of applications, the current consumption in sleep mode should be kept as low as possible. The RP604 consumes only 0.3 µA and has a peak efficiency of 90% at 0.1 mA output current.

RP511 100mA Buck DC/DC converter for IoT applications 

The RP511 is a VFM buck DC/DC Converters with synchronous rectification which can be powered from a coin cell to a USB port. The smallest solution requires only 8.0 mm2 PCB area including three external components. Therefore, this product is highly suitable for small wearable applications such as smartwatches, fitness trackers, RF modules, sensor devices etc. Current consumption is only 0.3 µA and peak efficiency is at 95% at 0.1 mA.

More information can be found in the links provided below:

https://www.e-devices.ricoh.co.jp/en/products/power/dcdc/rp604/

https://www.e-devices.ricoh.co.jp/en/products/power/dcdc/rp511/

        

 

Richardson RFPD join OEMsecrets

Richardson RFPD, an Arrow Company, is a global leading supplier in the RF and wireless communications, industrial IoT, power conversion and renewable energy markets.

Users can now search and purchase products from manufacturers such as MACOM, Analog Devices, Huber+Suhner, Sierra Wireless and Vincotech using OEMSecrets.com.

Peregrine Semiconductor’s newly released absorptive SP6T RF switch, is now in stock and ready to buy at Richardson RFPD through OEMSecrets.

Richardson - Peregrine Semiconductor part

With over 400 employees and more than 35 global locations, Richardson RFPD is dedicated to providing the latest products and technical expertise to support all aspects of customers’ go-to-market strategy, from prototype to production.

For further information, visit http://www.richardsonrfpd.com/

 

Counterfeit Avoidance – USNC/IECQ Distributor and Functional Testing Laboratory Advisory Group Development Update

The Distributors Advisory Group (DAG) is pleased to share the progress that is being made in the development of IECQ Counterfeit Avoidance in the USNC/IECQ Distributor and laboratory Advisory Groups.

Through the extraordinary efforts of Todd Kramer, Secure Components and the marketing and business development expertise of Julia Kocs, ECC Corporation, substantial progress has been made in the development of the USNC/IECQ DAG over the past 60 to 90 days.  As of today, 4 new members have been added to the USNC/IECQ IAB, three in the DAG and 1 in the Functional Test Labs, and relationships have been devleoped with GIDEP, ERAI, IDEA, Applied DNA Science, OEM Secrets, Net Components the DLA and others.

DAG have created a state-of-the-art Counterfeit Avoidance Mark Alliance (CAMA) website and begun the development of the Counterfeit Avoidance Mark Alliance and the Counterfeit Avoidance Mark Alliance Repository Management System, (CAMARMS).
Both the CAMA and the CAMARMS programs are getting very good reviews in the initial marketing outreach. www.counterfeitavoidance.org
The USNC/IECQ IAB and DAG are hosting a conference/meeting in Milwaukee WI from September 18th-20th. For more information please contact Christina Clark at the ECCC: christina.clark@ecccorp.org. At next weeks meetings, Todd and Julia will introduce two items for resolution by the DAG Membership, one will be the use of the new repository management system and the second, calling for the adoption by USNC/IECQ DAG Members to insist that their suppliers hold at least one of “IECQ Certification” plus IECQ ESD.

Depending on the supplier, acceptable IECQ Certifications would be one or more of the following:

Manufacturers Approval, (MA)
Technology Approval, (TA)
Hazardous Substance Process Management (HSPM)
Counterfeit Avoidance Process Management System (CAPMS) (This process approval program will be based on the IECQ QC 03-7 Rules of Procedure and SAE AS 6081 or AS 5553 as appropriate)
Automotive Qualification Approval (AQP)

Following the meetings next week, Press Releases will be sent out addressing these programs as well as brochures to help the Supply Chain find the resources they need for Training, Implementation and Certification.

For additional insight and ongoing information regarding the activities under way please visit the website, join DAG social media programs and visit the following links.

In this link you will find the banner ad posted on the ePartners page of OEM Secrets: http://www.oemsecrets.com/ourpartners.php
In addition to the shared marketing with OEM Secrets, DAG have also received a complimentary banner posting on the Net Components website.  http://www.netcomponents.com/.  This was in support of the September 6th Webinar hosted by Todd Kramer.  Together these two organizations represent membership of more than 4000 companies.

OEMsecrets.com, info@oemsecrets.com, www.oemsecrets.com

      

The USNC/IECQ DAG and the Functional Test Labs, Chaired by Mike Silverman, Ops Alacarte, will hold their first meetings in Milwaukee on September 18th and 19th and will participate in the other activities as appropriate.

Other Links that may be of interest.

http://www.adnas.com/
http://www.oemsecrets.com/ourpartners.php
http://www.netcomponents.com/
http://www.idofea.org/
http://www.dla.mil/Pages/default.aspx
Best regards,
Stanley H. Salot Jr. | President/CEO | ECCC
stan.salot@ECCCorp.org| Office: 541.847.0644 | Mobile: 510.773.4165 | Fax: 866.600.9008

ECC Corporation Web Site:www.ECCCorp.org

Compare the Market

Compare the market.

Ready for price comparision sites to hit the electronic component distribution industry?
OEMsecrets.com – This site gives great value to anyone buying electronic components. Would you sign up to a website and pay to search for where to buy your car insurance? At the moment in the electronics industry this is actually the case. Many sites charge an annual fee to the users before they are able to use the site to search. OEMsecrets is changing the way the industry searches for components as there is no sign in process, giving the user instant free access to view all the major distributors inventory for free. Distributors like Digi-key, Farnell,Newark,Avnet,Arrow and many more are all listing inventory on the site, with more and more suppliers uploading inventory every day.
That’s not all though, users are now wanting more and more- not only do they want datasheets and images and other information to help at the design stages,but they also want to know which suppliers have stock what the lead times are and how they are packaged. OEMsecrets is going even futher than this, shortly we will release a new version which will allow users to compare prices from the major distributors by quantity, simply entering a quantity to display the cheapest suppliers for the quantities they require.
In some cases parts may be obsolete /EOL. To help with this we have added a new independent supplier section on the site. This part of the site enables users to look at quality non-franchised distriubtors real in-stock inventory. We screen the suppliers to make sure they really have the inventory on their shelves and we don’t list any inventory from China. With these checks in place we can drastically reduce the chance of purchasing any poor quality/counterfit items. Should the user want to see more information about a supplier there is a page in which they can look at the suppliers information for any accreditations, ISO approvals etc.

Visit us for free @ www.oemsecrets.com

What’s happening in the electronic world

Electronics Distributors Online

DigiKey recently dropped their catalogue in favour of on-line sales. This is typical of the developments in the electronics distribution industry. All the major franchised distributors are trying to give the buyer all the tools they need in one easy to use website, even helping them to approve components at the design stage using sites like element14.
Buyers also want and expect more; they want live stock levels, pricing, packaging information like reel sizes etc.

OEMsecrets have listened to the major distributors and thousands of buyers from large OEM’s across the globe, and have developed a price comparison website where users can see millions of lines of inventory from all the major distributors with up to date stock levels, pricing etc. OEMsecrets is still developing the site further so the user will eventually be able to tailor the site to suit their specific requirements. Users will be able to send multiple requests to several distributors with just a few simple clicks. They will also be able to price thousands of items in just a few minutes using the BOM Machine, a tool that enables the user to upload their list of items. It then checks the items with the major distributors and returns the results with pricing and stock levels. The user can even price up the whole BOM in one currency even though the distributors may be in other countries.

Recently OEMsecrets have removed the log in and made the site 100% FREE for anyone to use. OEMserets have also split the search results screen so it displays both the franchised and non-franchised inventory separately. There are no distributors in China listed on the website. All inventory is in-stock only, no available stock is advertised on the website.
OEMsecrets is one of the fastest growing component sourcing websites online, with over 15 million line items of electronic components listed on the website. OEMsecrets lists global inventory feeds from the likes of DigiKey, Avnet, Arrow, Farnell, Future, Newark, Online Components etc and posts in-stock inventory from a number of independent distributors. OEMsecrets therefore caters for all active, passive, electro-mechanical and obsolete component requirements.

It’s OEMsecrets’ intention to give the user all the information they may possibly need on one free and easy to use website in order to find and buy electronic components: Our Website @ www.oemsecrets.com or about us @ About Us